Andrei Muntianu

MCF5211Demo flash programming problem, when using a notebook

Discussion created by Andrei Muntianu on Sep 2, 2008
Latest reply on Sep 15, 2008 by Tom Thompson
Hi,

I'm using a MCF5211Demo board, and when i try to write the program in flash using CF Flasher on a notebook I get the time-out error. This problem does not appear when I use a desktop.
Initially I thought it was a power issue, so I got a docking station, but I had the same problem, so I checked the USB voltage, and it was only 4.5V, so I got also a powered USB hub, now the voltage is 5V, it's stable , but the timeout issue is still present.

Can anyone suggest a solution?

Thankyou.

Muntianu Andrei Gabriel.

Outcomes