Hi,
I’m afraid that it is not possible to connect the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter, the reason is that the Digital interface input of the MC33814 is dependent from VCC voltage and VCC voltage should be 5V. Using a level shifter is the best solution for this case.
Have a great day,
Jose
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------