MX7 SABRE schematic: sim card connector J7 and SIM card signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX7 SABRE schematic: sim card connector J7 and SIM card signals

Jump to solution
663 Views
demoniacmilk
Contributor IV

hey there!

Id like to place an eSIM on an addon board for the MX7 SABRE.

Connector J7:

When I was looking for possibilities to connect the eSIM to the mx7 through the available connectors I stumbled upon the sim card connector (J7) in the schematic. It seems to be connected to the PCIe connector (J8) only? I cannot find the net respective labels anywhere else.

SIM card Signals:

SIM1P1 is part of the EPDC connector (EPDC_SD08..12). Simply connecting an eSIM to these pins (and adjusting the pin mux) should do the trick? Are there any drivers ready for (e)SIM cards under Linux?

Thanks,
Regards,
Lars

Labels (2)
0 Kudos
1 Solution
522 Views
art
NXP Employee
NXP Employee

Q. the sim card connector (J7) in the schematic. It seems to be connected to the PCIe connector (J8) only?

A. Yes. This SIM card is provided only for a wireless module to insert into the PCIe connector.

Q. Simply connecting an eSIM to these pins (and adjusting the pin mux) should do the trick?

A. Yes.

Q. Are there any drivers ready for (e)SIM cards under Linux?

A. Yes, the latest 4.1.15 Linux BSP provides the driver for the SIM interface module.


Have a great day,
Artur
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
523 Views
art
NXP Employee
NXP Employee

Q. the sim card connector (J7) in the schematic. It seems to be connected to the PCIe connector (J8) only?

A. Yes. This SIM card is provided only for a wireless module to insert into the PCIe connector.

Q. Simply connecting an eSIM to these pins (and adjusting the pin mux) should do the trick?

A. Yes.

Q. Are there any drivers ready for (e)SIM cards under Linux?

A. Yes, the latest 4.1.15 Linux BSP provides the driver for the SIM interface module.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos