Pin Connections for I2C interface with FXAS21002C and FXOS8700C sensors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Connections for I2C interface with FXAS21002C and FXOS8700C sensors

820 Views
akshayingle
Contributor I

Hi I am new to IMU sensors, I am using BRKT-STBC-AGM01 breakout board and trying to interface my MCU with the board. I am confused regarding the pin connections. 

first I am trying to interface Gyro sensor using I2C - FXAS21002C, later I will be interfacing FXOS8700C. 

The pin connections I have used for Gyroscope

Sensor Pin        MCU Pins

VDDIO                VDD

VDD                    VDD

SCL                    SCL 

SDA                   SDA

GND                  GND 

Am I missing anything else regarding pin connections? I haven't used interrupt pins yet. I want to operate the sensors in active mode. 

Kindly guide me 

Labels (2)
0 Kudos
1 Reply

475 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Akshay,

Please see below the schematic and pinout diagram.

Schematic.JPG

Pinout.JPG

So you need to connect the following pins to your MCU:

SCL1 - J3.4

SDA1 - J3.5

VDD_21002 - J3.7

VDDIO_21002 - J3.9

GND - J4.5

RST_21002 - J4.7 - connect to VDDIO_21002 if not used by your MCU

Note that the default 7-bit I2C slave address is 0x20 as SA0_MISO pin is tied to GND.

You might find useful also my simple bare-metal example project available here.

Hope it helps.

Best regards,

Tomas

0 Kudos