Hi,
I'm working on a project using imx6 Sabre Lite board. I want know how do I u-boot multiple imx6 Sabre Lite boards at the same time using one single Sd card and how to modify the MFG Tool code.
Regards
The current v.2.xx MFGtool software can service up to 4 devices at a time. You have to specify the number of simultaneously served devices as the PortMgrDlg parameter in the UICfg.ini file (located in the same directory as the executable file).
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Does it service 7-8 boards simultaneously?
No, no more than 4 boards.