AnsweredAssumed Answered

Mode configuration in eLBC for P1015

Question asked by Pavankumar G on Jul 19, 2017
Latest reply on Jul 19, 2017 by alexander.yakovlev

Hi,

 

I have a few queries with regard to the eLBC controller in the P1015. I have 3 devices connected to the eLBC bus which are - NOR Flash, FPGA and a NVRAM.   The NOR Flash is the boot device and is connected to the GPCM mode.

 

1.Can I connect all the three devices in the GPCM mode. Will it have any effect or will it create any problems while booting from NOR Flash.

 

2.Are there any limitations to connecting these three devices in the GPCM mode of the eLBC bus.

 

3.What mode of operation would be better for the FPGA and NVRAM - GPCM mode or UPM mode ?

 

How does one choose which mode needs to be used?

Outcomes