Sensor MPX2300DT1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensor MPX2300DT1

367 Views
joergmeier
Contributor I

Is the Freescale Pressure Sensor MPX2300DT1 produced and packed under clean room conditions? Which class of cleanroom? Is the sensor sterilized after production? Do you have any document, that cerifies the cleanroom production?

0 Kudos
1 Reply

263 Views
darioarias
NXP Employee
NXP Employee

Hello Joerg,

There is no documentation that certifies that the production of this part is made under clean room conditions and the part is no sterilized after production .This device have been designed with bio-medically approved materials with a history in medical situations to provide a sensor that can be used with confidence in applications, such as invasive blood pressure monitoring. It can be sterilized using ethylene oxide and it meets all USP XX Biological Testing Class VI requirements.

Darío

0 Kudos