AnsweredAssumed Answered

DDR Stress TEST, Freq range for OS

Question asked by Eishi Shibusawa on Jul 18, 2017
Latest reply on Jul 18, 2017 by Yuri Muhin
Branched from an earlier discussion

Dear Yuri

 

Thank you for your support.

 

It seems that the DDR CLK will be 528MHz, 24MHz or 10MHz when using NXP Linux BSP.

The range of DDR Stress TEST is from 135MHz to 672MHz.

Customer uses the DDR3-1066 (528MHz).

 

Q1.

Which range of DDR CLK should we evaluate by DDR Stress TEST Tool when using NXP Linux BSP.

 

Best Regards,

Eishi SHIBUSAWA

Outcomes