Hi,
I am working in Linux Yocto which is booting fine in i.MX6 based custom board. The Linux version is 3.14.38 The LCD is of low resolution 240x320. The BSP is actually made for 800x480 resolution LCD. The display clarity is just fine after booting . But the icons size is enlarged and all the application components seems to be displaced.
I tried with xrandr scale option but the touch does not seems to work in the scaled portion. Also scaling does not seems to be a better option because if I manage to make the matchbox to fit within the display area, the icons and font size is very very less , one can hardly manage to see them .
What is the best way to handle this issue. ? Where should I make change to make all the matchbox components to appear in a proper way.?
Thanks & Regards,
Anjali
Hi Anjali
for low resolutions lcd one needs to descrease frequency, please look
at suggestions on
Porting LVDS LCD With Low Resolution to i.MX6
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I had gone through the link provided . When we probed , the DISP_CLK is 7 Mhz. Since we are getting the pixel clock in a low range , I think then the clock must be fine.
Correct me if I am wrong.
Thanks & Regards,
Anjali
Hi Anjali
could you try latest bsps described on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for the reply. I have a couple of steps to follow according to our User Manual.
I believe, I have used the latest BSP from git using the below commands.
$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.38-6QP_ga
$ repo sync
Thanks & Regards,
Anjali
Hi Anjali
please try latest L4.1.15_2.0.0 described on
i.MX 6 / i.MX 7 Series Software and Development Tool|NXP
Best regards
igor
Hi Igor,
Our customer needs kernel version 3.14.38 only. Is there any display related known issue in linux kernel version 3.14.28?
Hi Anjali
since L3.14.28 many changes were made to sources, for ldb most important are
described in EB821 LDB Clock Switch Procedure & i.MX6 Asynchronous Clock Switching Guidelines
http://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf
Best regards
igor
Hi Igor,
We tried with an LCD of resolution 480x640. The issue doesnt appear here.