HI,
When i loading an module(insmod drv_ko), I am observing the below errors.
drv_ko: disagrees about version of symbol sock_create
drv_ko: Unknown symbol sock_create
drv_ko: disagrees about version of symbol sock_sendmsg
drv_ko: Unknown symbol sock_sendmsg
When i removed the CONFIG_NET_GIANFAR_FP from kernel config, i am not observing the above errors.
Is there any kernel config need to be defined to resolve the above issues other than CONFIG_NET_GIANFAR_FP config ?
Thanks,
Kamaraj
Hello Kamaraj,
Which version Linux Kernel do you use? I didn't find option "CONFIG_NET_GIANFAR_FP" in the recent release SDK Linux Kernel.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Yiping,
I was using 2.6.32.13 kernel from NXP LTIB
Thanks,
Kamaraj