Using CLRC663 without OS for the NFC Lib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using CLRC663 without OS for the NFC Lib

663 Views
michaelumundum
Contributor I

Hello,

I have to do a solution with the CLRC663 Reader IC which should work with Mifare Classic. Now my Problem is that the Lib is made that there should be an OS on the CPU. But the CPU is to small for a OS so I have to do it without an OS.

Do you have there some experience with this?

Is there a better docu which registers and command chains has to be used to work with Mifare Classic?

Thanks for some ideas.

0 Kudos
1 Reply

549 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Michael,

     Refer to Quick Start Up Guide RC663 Blueboard , please! See the link, please!

CLRC663 plus | multi-protocol NFC frontend|NXP .

    page 16:

Running the projects with, or without FreeRTOS

Hope above information can help you!

Have a nice day!

TIC Weidong Sun

0 Kudos