Hi,
I am working on a custom board which is based on i.MX6 solo board.Linux yocto is being used to boot the board . The kernel version is 3.14.38.The issue being faced is ,image size is larger.It is not fitting correctly on LCD.
LCD resolution is 320*240.
modified the dts file based on LCD datasheet.
i have seen the below thread, which tells change pll2 to pll5.
https://community.nxp.com/message/833716?commentID=833716#comment-833716
am not understanding where to change the clock to pll5.am not using sabre board.
Please suggest
Thanks and Regards
Rizwan Syed
Hello Rizwan,
Please follow the following document Porting LVDS LCD With Low Resolution to i.MX6 , In this document you can see that you need to modify the DTS file and also make some changes in the /arch/arm/mach-mx6/clock.c, there you can modify 3 ldb's clock source : &pll5_video_main_clk, &pll2_pfd_352M, &pll2_pfd_400M,
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------