AnsweredAssumed Answered

Regarding GDU confiuration to get phase votage using internal ADC channel

Question asked by PRATIBHA SURABHI on Jul 14, 2017
Latest reply on Jul 18, 2017 by Radek Sestak

HI,

 

I am using ZVMC128 MCU.
I am using internal ADC channel to calculate phase voltage.
So at one instant i will get only one phase voltage but i want all three phase voltages.
I have done the configuration of PMF,PTU,ADC,TIM0.
PMF reloads after each 50uS.
In that PMF reload ISR i am applying commutation pattern to GDU MUX register as follows

 

fsau8MuxPhase[7] = {0x00,0x03,0x02,0x01,0x03,0x02,0x01};

/* PMFCFG2 and PMFOUTC are configured as per output pattern */

GDUPHMUX_GPHMX = fsau8MuxPhase[outputPattern];
PTUC_PTULDOK = 1;

 

After applying commutation pattern to GDU MUX I will get the phase voltage for respective pattern on internal channel.

It is my understanding.
Is it right?

For UVW disconnection failsafe i have to check all three phase voltages.But i am not getting how to do this.

Please give me some solution.

Outcomes