AnsweredAssumed Answered

imx6ULL CAN Connection

Question asked by Soumya KS on Jul 12, 2017
Latest reply on Jul 13, 2017 by igorpadykov

Hi All,

 

I am using imx6.ULL EVK board. There is a CAN connector on the board which has pins for both CAN0(L/H) and CAN1(L/H).

 

I want to do a loop back from CAN0 to CAN1. How should I connect these pins? Is it enough if I just wire it up from L-L and H-H of Can0-Can1 respectively? There was a continuity seen in the other pins when I do that.

Is there a cable which can be procured anywhere particularly for this EVK?

 

Any leads will be of atmost help.

 

Thanks,

Soumya

Outcomes