Could BT.1120 support 1280x720@30fps YUV422 video output?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could BT.1120 support 1280x720@30fps YUV422 video output?

1,181 Views
takayuki_ishii
Contributor IV

Hi,

Patch to Support BT656 and BT1120 Output For i.MX6 BSP support both 1080p/i video output.

Could it support 1280x720 output video?

Labels (2)
0 Kudos
5 Replies

752 Views
takayuki_ishii
Contributor IV

Hello Diego

Thank you for your support.

I will answer it to my customer.

Best regards,

Ishii.

0 Kudos

752 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Thank you for writing.

Yes, it is verified working. The video data can be captured with BT1120 protocol.

Furthermore,It is SAV/EAV mode for 1280x720@30fps YUV422, not VSYNC+HSYNC mode.

I hope this can help you.

 

Best Regards,

Diego.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

752 Views
takayuki_ishii
Contributor IV

Hello Diego.

I have one more question.

Could BT.1120 support 1280x720@60fps YUV422 video output?

> Yes, it is verified working. The video data can be captured with BT1120 protocol.

Furthermore,It is SAV/EAV mode for 1280x720@30fps YUV422, not VSYNC+HSYNC mode.

Is this a result of video input?

I hope to know about 720p60 video output by bt1120 format.

Best regards,

Ishii.

0 Kudos

752 Views
diegoadrian
NXP Employee
NXP Employee

Yes, the code is ready. The only difference, is the clock frequency. The code is the same.

Best regards,

Diego.

0 Kudos

752 Views
takayuki_ishii
Contributor IV

Hello Diego

Thank you for your support.

Please teach me which environment do you use to test it?

If you use this patch https://community.nxp.com/docs/DOC-94019 

which point do you modify to test it?

If not, can we get a sample code or setting for it?

Best regards,

Ishii.

0 Kudos