Hello Experts,
I want to interface the below chip (FXOS8700) using SPI interface. It also supports i2c interface. In my imx6 board, I have interfaced this chip via SPI bus and want the driver for that.
I can find the FXOS8700 linux drivers for i2c interface but not able to find for SPI interface.
Any one can provide me the SPI driver for FX0S8700 chip?
Thansk for your support.
Regards,
Titus S.
Solved! Go to Solution.
Here is the driver for the FXOS8700 SPI interface.
fxos8700: add SPI driver · warpboard/linux-imx6@5ccf63f · GitHub
Hello Titus,
Thank you for writing.
Unfortunately, we do not have a Linux SPI driver for the FXOS8700. You can adapt the I2C driver that we provide, with the Linux SPI driver. The configuration will be the same, you only need to change the part of the I2C's communication.
I hope this can help you.
Best Regards,
Diego.
Here is the driver for the FXOS8700 SPI interface.
fxos8700: add SPI driver · warpboard/linux-imx6@5ccf63f · GitHub