Benjamin Heder

Is the SPI program provided by the FRDM-K66's SDK supposed to work?

Discussion created by Benjamin Heder on Jul 12, 2017
Latest reply on Aug 8, 2017 by Benjamin Heder

Hello everyone,

 

I am working with MCUXpresso and I have an issue with the SPI program "dspi_interrupt_transfer" provided by the FRDM-K66's SDK.
Actually when I debug it and try to look inside the SPI0 and SPI1 registers these ones remain disabled in Memory -> Monitors Window.

Then I try with the SPI program "dspi_polling_transfer" and once again it doesn't work.

 

Is there a bug in DSPI SDK examples?

 

Do you have any solution for this problem because I run out of idea.

 

Best Regards

 

Ben

Outcomes