AnsweredAssumed Answered

S-function compiling issue with AMCLIB

Question asked by Ruonan Zhou on Jul 11, 2017
Latest reply on Sep 19, 2017 by Ruonan Zhou

Hello,

 

We are using the AMCLIB(Automotive and Motor Control Library) in our application code in C, and trying to develop a SIL testing the application code. We use a S-function in Simulink to call the application code. However, the library seems to be written in assembly and when we included the library for the s-function, Matlab had compiling issue with the library.

I'm wondering if the library actually can be run on a windows machine since it's in assembly, and if there's a way to use AMCLIB in SIL.

 

Thank you very much:)

 

Ruonan

Outcomes