Dear NXP,
I used K64 CPU with MQX4.1, When I used UART in my project, baud rate is setting to 115200, and the issue is if I set the parity to odd, the even/odd parity of my software can both connect to my device which is k64.
and if I set the device parity to even, the odd/even parity of my PC software can both connect to the device too.
Can you show me what's the problem, I think it is bsp of the mqx4.1 issue.
BR,
Hi wulin:
I would suggest you check the UARTx_C1 register to get the real value for parity check first.
Regards
Daniel
Dear Daniel,
Thank you for your reply, and I have checked the UARTx_C1 register:
ODD: 0x13
EVEN: 0x12
It seems right, but when I do the test, it is the same when setting even or odd.
BR,