AnsweredAssumed Answered

The Battery is powered by 24V,MC33978 switch detection range

Question asked by Jack Jiang on Jul 10, 2017
Latest reply on Oct 24, 2017 by Jack Jiang

Dears,

 

咨询下:关于MC33978开关检测芯片。如果Battery 采用24V供电,SP0配置为检测高,SP0 输入5V能检测到吗?

 

If the Battery is powered by 24V and SP0 is configured to detect high. Can SP0 detect the input 5V is high level?

Outcomes