LIN Question about S32K144EVB-Q100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LIN Question about S32K144EVB-Q100

769 Views
jinhui_wu
Contributor III

I am testing LIN example in S32DS on S32K144EVB-Q100.

File->New->New S32DS project from example,then find S32K144 RTM SDK v1.0.0 Example Projects,open lin_master project.

builded ,complied,debuged,then un-plug USB cable.power on from 12V and reset the MCU.

I use Oscilloscope to look the wave of LIN pin and tx on TJA1027,I find wave is working.LIN is communicating.

Now I short LIN pin to GND for one second,at this time the wave of LIN pin lose,the wave of tx on TJA1027 lose.

when i don't short LIN pin to GND, LIN still can't work.

why?

after LIN pin is shorted GND for one second,then LIN pin isn't shorted GND.Would LIN still work as usually?

Labels (1)
0 Kudos
0 Replies