Multiplexed address/data bus (IFC_AD0-AD15) of the LS1043A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiplexed address/data bus (IFC_AD0-AD15) of the LS1043A

Jump to solution
1,233 Views
danmoffatt
Contributor II

Can the multiplexed address/data bus (IFC_AD0-AD15) of the LS1043A be connected directly to the data bus of a NOR Flash device and also to the input of a latch device to latch the addresses for the NOR Flash device?

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,031 Views
danmoffatt
Contributor II

Thank you! I assumed that but somehow didn't find the info in the manual.

View solution in original post

0 Kudos
2 Replies
1,032 Views
danmoffatt
Contributor II

Thank you! I assumed that but somehow didn't find the info in the manual.

0 Kudos
1,031 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes the multiplexed address/data bus (IFC_AD0-AD15) of the LS1043A can be connected directly to the data bus of a NOR. See example from the reference manual.

pastedImage_1.png

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos