AnsweredAssumed Answered

s32k144 FTM_SignalMeasurement_Example can not work

Question asked by 博 姜 on Jul 11, 2017
Latest reply on Jul 12, 2017 by Petr Stancik

i use the example to  test but can not work ,i did not connect error the line ,two line is pTC0 and PTB2,

 

when I test I find it could not into the interrupt,I change the PORT of the INPUT ,it can not work

 

it have PWM out ,but the input part can not work,

 

what is the problem, i am crazy,could you help me

Outcomes