AnsweredAssumed Answered

The LCD maximum resolution for i.MX6 SoloLite.

Question asked by George Fukutomi on Jul 10, 2017
Latest reply on Jul 10, 2017 by igorpadykov

Dear All,

 

My customer has planned the Digital Signage product using i.MX6 SoloLite.
They will use 24bit 1280 x 800 LCD.

 

I checked the data sheet and reference manual for SoloLite.
And I have found that there is a description which is different in each.

 

DS: Page 4.

  LCD, 24-bit display port, up to 225 Mpixels/sec (for example, WUXGA at 60 Hz)

 

RM: Page 131.

  LCDIF supporting one parallel 24-bit LCD display with up to WXGA(1366x768)
  resolution at 60 Hz

 

Which is correct?

 

BR,

George

Outcomes