AnsweredAssumed Answered

I am using the K64F with an attached JY-MCU (HC-05) as a master.

Question asked by elinaiman on Jul 10, 2017
Latest reply on Jul 13, 2017 by Hui_Ma

The slave is an android tablet. I am also using 2 IO lines on the K64F to connect to the EN and STATE lines on the HC-05.

When the slave shuts down, the master detects that via the STATE line on the HC-05. However when the slave starts up again, the HC-05 does not re-link to it automatically. I know that if you put the power OFF and then ON on the HC-05 it will re-connect.

On the K64F (J199) the power to the JY-MCU is connected directly to 3.3V line and not an IO line.

Do I have to use an IO line for the power.

Is there another procedure to get the JY-MCU to auto-connect without turning off the power. 

Thanks for your help.

Eli Naiman

Outcomes