Hi Guys,
(1)There are some question about the Force out Logic,the Figure 25-17.Force Out Logic in MPC5643L Microcontroller
Reference Manual page672.shown as below:
1#:Abve Figure ,the Part A,there is a box that label D ,Force_Out and Q, the relationship between the three?
(2) in MPC5643L Microcontroller Reference Manual page708,shown as below:
2#:the content said the register(SWCOUT) is used to set the deadtime,i have some doubt to be confrimed,
2.1:How the deadtime is achieved ? I thought If We set the SWCOUT to 0,When the Q output the value 2,and the Mux output the OUT23-3=0,then the deadtime is achieved.
for exzample:
frist,We set the SEL23_3 =10,then OUT23_3 will insert the deadtime ;
second,IF we set OUT23_3 =0,and the deadtime Zero will be insert,if we set OUT23_3 =1,the he deadtime one will be insert? is that right ?
2.2:is PWM23 is equal to PWMA,And PWM45 is equal to PWMB?
I don't know the PWM23_3 corresponds to which pin of the hardware?
Thank you !