AnsweredAssumed Answered

Discrepancy about GPIO1[5] & GPIO1[15] of P1022

Question asked by Cagatay Kalelioglu on Jul 6, 2017
Latest reply on Jul 12, 2017 by Cagatay Kalelioglu

Hello,

 

There is a discrepancy about GPIO1[5] and GPIO1[15] of P1022 between its application note AN4343 and its datasheet and reference manual.

 

Datasheet and Reference Manual: The pin TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK (Package pin number: AC26) is GPIO1_5:

 

Application Note (AN4343):  The pin TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK is GPIO1_[15]:

 

Reference Manual again: The pins TSEC_1588_CLK_OUT and TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK are both shown as GPIO1[15] in the figure of signal groupings:

But, the pin  TSEC_1588_CLK_OUT's alternate function is given as GPO1[15] two pages after the figure:

 

My guess is:

TSEC2_TX_CLK/USB2_CLK/TSEC2_GTX_CLK -> GPIO1[5]

TSEC_1588_CLK_OUT -> GPO1[15]

 

Could you confirm?

 

Best Regards,

 

Cagatay Kalelioglu

Outcomes