MPC5746C ISO CANFD NOT WORKING

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C ISO CANFD NOT WORKING

618 Views
akshay_hv
Contributor I

Hello,

I developed the CANFD driver for MPC5746C MCU . It is working fine CANOE if we select the NON ISO CAN FD option in CANOE tool.
But It is not working if we select the ISO CANFD. I tried to find information of configuring this in the code. I didn't find much information on this.

please clarify the point whether the micro will support ISO CANFD .. If so how to configure the same.

Regards

Akshay H V

Tags (2)
0 Kudos
1 Reply

501 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure you are using the MCU with the maskset 0N84S or 1N84S. Those MCU cuts implements ISO CAN FD protocol.

Previous masksets are not compliant with ISO CAN FD, refer to erratas http://www.nxp.com/docs/en/errata/MPC5746C_1N06M.pdf.

BR, Petr 

0 Kudos