Can we use latest Bug fix tag for Android 6.0.1 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use latest Bug fix tag for Android 6.0.1 ?

604 Views
ThanarajS
Contributor III

Hi All,

   We have doubt that, can we use latest Marshmallow android bug fix source code commit TAG for android 6.0.1 setup ?... In android Marshmallow user guide they have mentioned below link for repo init,

$ ~/bin/repo init -u https://android.googlesource.com/platform/manifest -b android-6.0.1_r22

Please let us know, can we use updated Tag for Android 6.0.1 ? if yes please tell latest tag number.

Regards,

Thanaraj.

Regards,
Thanaraj Subramani
0 Kudos
3 Replies

437 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Thanaraj ,

Yes,  you can use the bug fix source code commit TAG for Android 6.0.1  we have tested to

https://android.googlesource.com/platform/frameworks/av/+/refs/tags/android-6.0.1_r58, which is on marshmallow-mr2-release. It's also newer than our android_M6.0.1_2.1.0 release.

But I do not see a problem to use the latest R8.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

437 Views
bhaveshmoradiya
Contributor II

Hi,

I have same issue qemu-kernel.

fatal: bad object f7cfc2cca15736862e45ebef54776e0dfdffeb16
Error! Base version commit f7cfc2cca15736862e45ebef54776e0dfdffeb16 doesn't exist in git /home/<user>/myandroid/prebuilts/qemu-kernel. Stop

I an working on M6.0.1_2.1.0 R3 Please Help me what I'm Missing or did wrong.

I already spend too much time on this.

Thanks.

0 Kudos

437 Views
ThanarajS
Contributor III

Hi Jamesbone,

Thanks for reply.

As you said we have tried Tag r58 and r8, after repo sync whlie running c_patch for the android source bsp(android_M6.0.1_2.1.0), we are getting the following error.

Checking KEEP project - prebuilts/qemu-kernel ...
fatal: bad object f7cfc2cca15736862e45ebef54776e0dfdffeb16
Error! Base version commit f7cfc2cca15736862e45ebef54776e0dfdffeb16 doesn't exist in git /work/myandroid/prebuilts/qemu-kernel. Stop

Did you get any error like this while testing tag r58. can you please provide suggestion to solve the above error ?

Regards,

Thanaraj.

Regards,
Thanaraj Subramani
0 Kudos