Reading a file from "flash disc"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading a file from "flash disc"

701 Views
igormasár
Contributor II

Hello, I use S32K144 when I connect the device through the USB cable to the computer, it is recognized as a flash disc. So I would like to exploit this feature to an user can store here a configuration file. How can I read the file via the S32K144 ? I tried if the fopen is implemented unfortunately not. I do not want to use some other libraries such as EAR SDK. Is it possible to read the file ? Could you get me an example? Thank you in advance.

Labels (1)
0 Kudos
1 Reply

569 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I don't think you can read the flash disk with S32K.

This is OpenSDA Interface.

Regards,

Daniel

0 Kudos