Interrupt-problem with s32k144 devkit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt-problem with s32k144 devkit

Jump to solution
1,143 Views
lukasschäfer
Contributor III

Hello Community,

i have a problem with the example "FTM Edge Capture" from the Model Based Design Toolbox v2.0 for s32k144.

I connected PTC0 to PTC 15 and measured a PWM.

But the Interrupt service routine is not executed. The LED shines red all the time without blinking.

Thanks for support.

Original Attachment has been moved to: ftm_input_capture_s32k14.mdl.zip

0 Kudos
1 Solution
929 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi lukasschäfer‌,

If you own a S32K rev1.0 board then please use the Model Based Design Toolbox rev1.0 to program the board.

You can download it from here: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7296847 

Please use the examples from that toolbox.

You should expect this:

1.JPG

2.JPG

Hope this helps!

Daniel

View solution in original post

2 Replies
929 Views
lukasschäfer
Contributor III

Thank you Daniel.

This is the solution.

Lukas

0 Kudos
930 Views
dumitru-daniel_
NXP Employee
NXP Employee

Hi lukasschäfer‌,

If you own a S32K rev1.0 board then please use the Model Based Design Toolbox rev1.0 to program the board.

You can download it from here: https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7296847 

Please use the examples from that toolbox.

You should expect this:

1.JPG

2.JPG

Hope this helps!

Daniel