AnsweredAssumed Answered

Kea Bootloader AN5400

Question asked by martinodeluca on Jun 30, 2017
Latest reply on Jul 12, 2017 by Mark Butcher

Hello Guys, I am trying to use the Bootloader PC software and firmware from nxp AN5400 and i have some problems. The software PC works quite well but i have problems when I upload by means of Application a new firmware (I used one of an example of SDK frdm.128 and freedom board FRDM-128). The problems is that the new firmware doesn't work even if the procedure is correct. I noticed that if I launch from debug (s32) the application firmware, it works very well. I'am going mad because i can't explain this behavior. The firwmare is present from the address 0x1000  f MCU but it doesnt' work.

 

Someone have experienced with this problem?

 

Martino

Outcomes