AnsweredAssumed Answered

Adding a file/folder in rootfs nxp yocto build

Question asked by RAM MURMU on Jun 28, 2017
Latest reply on Jul 2, 2017 by RAM MURMU

Hi ,

   I am trying to add a file in rootfs so that the subsequent built image contain the added file/folder. I am performing the following steps -

 

1. Adding an entry for file in base-files_3.0.14.bb

 

2. Keeping corresponding file under ../poky/meta/recipes-core/base-files/base-files/

 

3. bitbake -c compile base-files

 

4. bitbake fsl-image-minimal

 

I am getting the following error -

 

ERROR: QA Issue: non debug package contains .debug directory: base-files path /work/p1022ds-fsl-linux-gnuspe/base-files/3.0.14-r86/packages-split/base-files/.debug/test_i2c_p1022
ERROR: QA run found fatal errors. Please consider fixing them.
ERROR: Function failed: do_package_qa
ERROR: Logfile of failure stored in: /home/ram/POTP/SDK-V1.8/QorIQ-SDK-V1.8-20150619-yocto/build_p1022ds_release/tmp/work/p1022ds-fsl-linux-gnuspe/base-files/3.0.14-r86/temp/log.do_package.8502
ERROR: Task 747 (/home/ram/POTP/SDK-V1.8/QorIQ-SDK-V1.8-20150619-yocto/poky/meta/recipes-core/base-files/base-files_3.0.14.bb, do_package) failed with exit code '1'

 

What is the problem and how to rectify it.

 

Regards

Ram

Outcomes