Hello,
What is the actual location of i.MX6 internal thermal sensor ? How the temperature values are different from Tj. What are the recommended safe limits of temperature to throttle down the frequency or shutdown the processor?
Hi Himanshu
thermal sensor is described on app notes :
AN5215 i.MX 6 Temperature Sensor Module
http://www.nxp.com/docs/en/application-note/AN5215.pdf
AN4579 i.MX 6 Series Thermal Management Guidelines
http://cache.nxp.com/docs/en/application-note/AN4579.pdf
Actual location of i.MX6 internal thermal sensor is not available,
one can consider that it measures Tj.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------