Hi sburck,
I hope you solved your problem but still are somewhere around here.
We are haveing the same or similiar issue with our board runnning a MPC5200B.
We are using one SDRAM (MT48LC16M16A2-75 , 16bit Databus , 66MHZ)
When we connect a debugger (Lauterbach) and are looking at a memory dump of the SDRAM, we see
some bits toogling around. The toogling is only if we read out the memory with 32 bit bursts (2 bits on each DQ per read), not with 16 bit bursts. Also the toggling only happens on the low nibble of the upper 16 bits, but not in every 32 bit Word. (bits marked with x ---0000 xxxx 0000 0000 ).
Looking at the signals with an oszilloscope the slew rate / Tsetup and Thold seems to be ok.
Attached you can find two pictures of the command signbals + one Data Signal DQ8
If you have any idea I'd appreciate your input.
Thanks, Daniel
I was surprised to see this thread still alive - that project was years ago. The lines for the RAM were the problem - they were OK for the SDRAMs in the original project, but the DDRAM that replaced them were flaky because of ringing. After redoing the card with shorter lines the problem went away.