Hi
I'm looking for AMR characteristisc for GPIO pins of IMX6Q.
Particularity I'm interested how much current can GPIO output absorb.
I connected the output of GPIO through resistor to another output P1, so that of P1 forces voltage it "wins" , if P1 is HighZ then GPIO forces the line.
if P1 forces 3.3v but GPIO pulls to 0v then GPIO takeas current of 3.3V/R , what is the allowable current?
Bar.
Hi Bar
typical current can be estimated using sect.4.8.1 GPIO Output Buffer Impedance
i.MX6DQ Datasheet
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
Unfortunately max. current is not specified.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------