AnsweredAssumed Answered

Image flickering problem after running the application program

Question asked by RAMANJINEYULU THOTA on Jun 26, 2017
Latest reply on Jun 28, 2017 by igorpadykov

Hi,

 

I am currently working on image flickering problem. I am using "galcore" kernel module and running the application of triangle shape. When i have run the application the image starts flickering.

I could not understand the problem in GPU driver and video driver.

 

In application we can use sleep() function to avoid the flickering issue, but if we want to run multiple applications we could not use the sleep() function.

Issue: I suspect the issue with GPU usage is increase then video driver starts to flickering but in GPU driver where exactly i have to find the GPU usage is increasing or not.

 

Could you please help on this to change the GPU driver to avoid the flicking issue.

 

Thanks in advance.

 

Thanks & Regards,

Ramanjineyulu.

Outcomes