AnsweredAssumed Answered

Gstreamer not working with imx53 custom board

Question asked by Prasad Roy on Jun 26, 2017
Latest reply on Jun 26, 2017 by igorpadykov

I am using the mfw_isink plugin for gstreamer for video streaming.

I have set the local alpha feature as export VSALPHA=1 and launch the gstreamer using below command.

 

gst-launch mfw_v4lsrc  device=/dev/video0  ! mfw_isink

 

I am seeing only colored lines in the display and  not able to stream the video.

 

The log details are given below.

  

MFW_GST_V4LSRC_PLUGIN 2.0.3 build on Jun 15 2017 10:07:07.

set color key

MFW_GST_ISINK_PLUGIN 2.0.3 build on Jun 15 2017 10:06:49.

Setting pipeline to PAUSED ...

In MVC:mxc_streamoff

 

 In MVC:mxc_streamon

IPU:In csi_enc_enabling_tasks

In csi_enc_setup

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

can not create threadmfw_gst_isink_setcaps:1390

VS0 created. in fmt[I420] win(0,0-mxc_ipu mxc_ipu: Channel already disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

176,144:176x144).

mxc_ipu mxc_ipu: Channel already disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

Outcomes