AnsweredAssumed Answered

Can't find I2S MCLK source options in K22F documentation

Question asked by MILLER on Jun 26, 2017
Latest reply on Jun 27, 2017 by MILLER

The MK22FN1M0AVLH12 reference manual's section on the I2S module master clock says to see the chip-specific configuration information for the definitions of the input options used by I2Sx_TCR2[MSEL] and I2Sx_MCR[MICS].  I can't find those definitions in the chip-specific information - just the rather unhelpful statement that "The MCLK Input Clock Select bit of the MCLK Control Register (MCR[MICS]) selects the clock input to the I2S/SAI module’s MCLK divider."

 

Where are these clock source options listed?

 

Thanks,

 

Scott

Outcomes