AnsweredAssumed Answered

ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010013

Question asked by sharath kumar on Jun 26, 2017

Hi,

i am working custome p2040 board. I am tryting to get hello_reflector application working on our board.

 

CPU0: P2040E, Version: 1.1, (0x82180011)
Core: e500mc, Version: 2.2, (0x80230022)

 

SDK version is 1.6

kernel is Linux-3.8.13-rt9+

Fman1: Uploading microcode version 106.1.11

 

 

i am gettting the below error when i run fmc application

 

sh-4.3# ./fmc -c config_1g.xml -p usdpaa_policy_hash_ipv4.xml -a
ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010013
sh-4.3#

 

below is the content of condif_1g.xml file

<cfgdata>
<config>
<engine name="fm0">
<port type="1G" number="0" policy="hash_ipsec_src_dst_spi_policy0"/>
</engine>
</config>
</cfgdata>

 

in the kernel cmd line i am passing "bootargs usdpaa_mem=64M ..." and the dts file is attached

 

Request to help me in solving this issue

 

Regards

Sharath

Original Attachment has been moved to: testdpaa.rar

Outcomes