i.MX6 Die revision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Die revision

584 Views
JamesMcCann
Contributor I

Hello. The latest i.MX6 Obsolescence notice affects the MCIMX6G2CVM05AA. Hello. 

MCIMX6G2CVM05AB is listed as the correct replacement. Could you please let me know what the differences between these die revisions are?

Tags (1)
0 Kudos
1 Reply

408 Views
igorpadykov
NXP Employee
NXP Employee

Hi James

difference is fixed erratum ERR010690 : SNVS LP (backup battery domain) reset bug during 

power up / power down, rev 1.2 part numbers will be identified with a “B” suffix.

One can refer to i.MX6UL Errata
http://cache.freescale.com/files/32bit/doc/errata/IMX6ULCE.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos