Booting from SD card on t2080RDS board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting from SD card on t2080RDS board

426 Views
matiaslirman
Contributor II

Hello,

I have downloaded the 'QorIQ Linux SDK v2.0 PPC64E6500 IMAGE' from NXP and have burned it onto an SD card adn placed it in the board and I have switched the switches to the appropriate setting, found on the quick start guide but when I turn on the board I do not see anything on the serial port connection. IS there something else I have to do in order for the board to boot from SD? Are there some lines of code I should implement into normal operation first? Any help would be appreciated!


Mat

Labels (1)
0 Kudos
1 Reply

288 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> have burned it onto an SD card

Please provide log of this operation.

What is the complete board name?

Please provide U-Boot log for NOR booting.

0 Kudos