Hi,
I'm using an nxp imx6ullevk board with murata 1DX evk (chipset BCM4343W), murata imx interconnect v2 wifi over sdio. Buildroot is using to build the final image for the board. I need to test the wifi and the bluetooth connections but i don't know where the broadcom tools can be downloaded. Where can i get the wl and bluetooth testing tools?
I have an issue while trying to enable the wifi. I can't get any ip address on wlan0 interface. I've got those error messages :
# ifconfig wlan0 up
Dongle Host Driver, version 1.141.92 (r)
Compiled in drivers/net/wireless/bcmdhd
wl_android_wifi_on in
mmc0: queuing unknown CIS tuple 0x80 (2 bytes)
mmc0: queuing unknown CIS tuple 0x80 (3 bytes)
mmc0: queuing unknown CIS tuple 0x80 (3 bytes)
mmc0: queuing unknown CIS tuple 0x80 (7 bytes)
mmc0: queuing unknown CIS tuple 0x80 (3 bytes)
mmc0: queuing unknown CIS tuple 0x80 (6 bytes)
F1 signature OK, socitype:0x1 chip:0xa9a6 rev:0x1 pkg:0x3
DHD: dongle ram size is set to 524288(orig 524288) at 0x0
dhdsdio_write_vars: Download, Upload and compare of NVRAM succeeded.
dhd_bus_init: enable 0x06, ready 0x06 (waited 0us)
wifi_platform_get_mac_addr
Firmware up: op_mode=0x0005, MAC=60:f1:89:3c:32:d8
Firmware version = wl0: Dec 11 2014 04:20:45 version 7.10.323.34 (r520360) FWID 01-ea2beeba
dhd_wlfc_init(): successfully enabled bdcv2 tlv signaling, 79
dhd_wlfc_init: query wlfc_mode succeed, fw_caps=0x1c
dhd_wlfc_init(): wlfc_mode=0x1c, ret=0
CFG80211-ERROR) wl_update_wiphybands : error reading vhtmode (-23)
wl_create_event_handler(): thread:wl_event_handler:7541 started
CFG80211-ERROR) wl_event_handler : tsk Enter, tsk = 0x884e143c
Did somebody already have this issue? While can't i get an ip address on wlan0? What are the steps to follow to have the board working well? Which kernel configurations are mandatory?
Thank you for your support