AnsweredAssumed Answered

Problem in LPC18LPC43InternalFLASHBootResetscript.scp

Question asked by Udo Eberhardt on Jun 23, 2017
Latest reply on Jun 29, 2017 by Udo Eberhardt

I found that the debugger does not work as expected with LPC4333 and LPC-Link2. The CPU does not get reset when I start a debug session. This turned out to be a problem in the debugger script LPC18LPC43InternalFLASHBootResetscript.scp. The script contains these two statements which are inactive, though.

 

160 REM cmresetvectorcatchset this
170 REM cmvectresetreq this

 

If I remove the REM from both lines then the debugger works as it did before with LPCxpresso.

Can someone confirm this to be an issue in MCUXpresso?

 

Version info: MCUXpresso IDE v10.0.0 [Build 344] [2017-03-21] 

 

Thanks

Udo

Outcomes