i.MX7 industrial temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 industrial temperature

512 Views
ssinfod
Contributor IV

Hello, the i.mx7 has very nice feature and specification.

However, I notice that the operation temperature are: -20 to 85 Celsius.
Typically, industrial CPU have more wider range : -40 to 85 Celsius.

Why the i.mx7 is limited to -20 instead of -40 ?

Is there any plan to provide a -40 version in a near future ?

Phil D

0 Kudos
1 Reply

377 Views
b36401
NXP Employee
NXP Employee

We are no plans for i.MX7 processors for -40C at this moment.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos