After some burnnings my MCU stopped responding. Giving the following error:
Connecting to J-Link ...
J-Link is connected.
Firmware: J-Link ARM V7 compiled Jun 20 2012 19:45:53
Hardware: V7.00
S / N: 157001692
OEM: IAR
Checking target voltage ...
Target voltage: 5.12 V
Listening on TCP / IP port 2331
Connecting to target ... ERROR: Kinetis (connect): Timeout while halting CPU. CPU does not stop.
ERROR: Kinetis (connect): Timeout while halting CPU. CPU does not stop.
Any idea what's going on?