AnsweredAssumed Answered

Need help with PN7462 configuration

Question asked by Bojan Jovanovic on Jun 20, 2017
Latest reply on Aug 10, 2018 by xubin xu

Hello guys,

 

In my current project, I'm using PN7462 module from NXP. I need that module for the following:

 

1. To communicate with NFC card

2. To communicate with GSM module via UART interface. I need to have 1.8V level UART communication with GSM unit. Configuration commands for GSM should be sent from PN7462 to GSM. 

3. To control a few of the GPIO signals.

 

I'm reading PN7462 datasheet but I'm not sure I can digest it in a way to properly design my board. Would you guys be so kind to help me with the following:

 

1. How to supply the PN7462 module? Which power pins do I need to connect to power supply? How to achieve 1.8V for UART and GPIOs?

2. How to download the firmware on PN7462? Using SWD interface ?

3. How to properly design the antenna circuit for NFC communication. Is there any antenna chip available on the market or I need to print it on a PCB?

 

Thank you very much for your time and effort. Really appreciate it.

Looking forward to reading from you.

 

Sincerely,

Bojan.

Outcomes