AnsweredAssumed Answered

How to do pin muxing on Freedom Ls1012A

Question asked by shyam baldha on Jun 19, 2017
Latest reply on Sep 25, 2017 by ufedor

Hello Community,


Do we have only 'QorIQ Configuration and Validation Suite'  is the option to do pinmux on freedom LS1012A board ??


Can't we do the pin muxing as of its been done over all iMX platforms??


For Example: 



If I wants to configure a pin as GPIO which is configured as UART by default, The only thing I have to do on iMX platform is to change the muxing MACROs as below:  


pinctrl_uart1: uart1grp {            
fsl,pins = <    

     MX6QDL_PAD_SD3_DAT7__UART1_TX_DATA  0x1b0b1

     MX6QDL_PAD_SD3_DAT6__UART1_RX_DATA  0x1b0b1




pinctrl_uart1: uart1grp {

fsl,pins = <

       MX6QDL_PAD_SD3_DAT6__GPIO6_IO18        0x1b0b1

       MX6QDL_PAD_SD3_DAT7__GPIO6_IO17        0x1b0b1        



So is it possible to do the pinmuxing in a same way on FRDM-LS1012A  board?? If yes Please provide the proper documentation if not please Guide me on the other way to do pinmuxing on FRDM-LS1012A with proper documents.