hello:
i intergrated the freemaster codes into my application code,and download the S19 file into the evaluation bord.
the communication configuration is :
(1)short-inter mode;
(2) the FMSTR_Poll() is in for(;;),FMSTR_Isr() is in can receive interrupt function; FMSTR_Init();
(3)FlexCAN, SPC56**
Then, the result of “Test Connection”:
" target is alive (responded to ping)"
the standard frame 0x7aa send and the response is received,but in the next step i click the button " STOP " to start communication,the results is below:
" Can not detec the board information! the communication will paused. Error code: 0x858e0003
I have several questions:
(1) Freemater through CAN, the protocol of communication is XCP/CCP? because i do not find the protocol in the specification,please confirm the information。
(2) without can protocol,how can i fix the problem?
looking forward to your response,My E@mal is" flesher@126.com ", thank you.