Is there any way to detect the reset source of the LPC1785 mcu?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any way to detect the reset source of the LPC1785 mcu?

840 Views
hongjianzhang
Contributor III

Recently many our boards didn't work well, the phenomenon is some board began to reset all the way when the MCU is  first in deep sleep mode and second wake up from IO then third we use the watchdog illegal command to reset the MCU to reset all our application.  we want to make sure which of the reset source lead to the mcu reset.

Labels (1)
Tags (3)
0 Kudos
1 Reply

520 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread

Internal RAM to determine cause of core reset 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos